Write/Read
See Fail Limit Lines

RedTraceOnFail Property


Description

Set and return whether to display limit line failures as red trace segments or red data points (dots).

 VB Syntax

pref.RedTraceOnFail = bool

Variable

(Type) - Description

pref

A Preferences (object)

bool

(Boolean) -  Choose from:

False - Display failures as red data points (dots).

True - Display failures as red trace segments. (Red Trace On Fail).

Return Type

Boolean

Default

False

Examples

pref.RedTraceOnFail = False 'Write

prefer = pref.RedTraceOnFail 'Read

C++ Syntax

HRESULT put_RedTraceOnFail( VARIANT_BOOL bValue)

HRESULT get_RedTraceOnFail( VARIANT_BOOL *bValue)

Interface

IPreferences10