Read-Only
About SA Application

ResBWList (Spectrum Analyzer) Property


Description

Read the list of all Resolution Bandwidth values currently supported with spectrum analyzer current settings.

VB Syntax

sa.ResBWList = value

Variable

(Type) - Description

sa.

A SpectrumAnalyzer (object)

value

(Variant)  Variable to store the returned Resolution Bandwidth values.

Return Type

Variant array

Default

N/A

Examples

value = sa.ResBWList 'Read

C++ Syntax

HRESULT get_ResBWList(VARIANT* resolution);

Interface

ISpectrumAnalyzer5