Read-only
About SA Application

ResolutionBWMax


Description

Read the maximum resolution bandwidth.

VB Syntax

value = sa.ResolutionBWMax

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

Return Type

Double

 

value = sa.ResolutionBWMax 'Read

See an example program.

C++ Syntax

HRESULT get_ResolutionBWMax(tagNASAResolutionBWMax* maxbw);

Interface

ISpectrumAnalyzer