| Read-Only | About SA Application | 
| Description | Read the DFT resolution. | 
| VB Syntax | sa.dft.Resolution = value | 
| Variable | (Type) - Description | 
| sa.dft | A SpectrumAnalyzerDFT (object) | 
| value | (Double) Variable to store the returned DFT resolution. | 
| Return Type | Double | 
| Default | N/A | 
| Examples | value = sa.dft.DFTResolution 'Read | 
| C++ Syntax | HRESULT get_Resolution(double* resolution); | 
| Interface | ISpectrumAnalyzerDFT |