Write/Read |
About Gain Compression |
Description |
Set and read the reverse power level to the DUT. This is applied to the DUT output port when making reverse measurements like S22. |
VB Syntax |
gca.ReverseLinearPowerLevel = value |
Variable |
(Type) - Description |
gca |
A GainCompression (object) |
value |
(double) Reverse power level in dBm. Choose a value from +30 to (-30). |
Return Type |
Double |
Default |
-5 |
Examples |
gca.ReverseLinearPowerLevel = -10 'Write |
LinPwr = gca.ReverseLinearPowerLevel 'Read |
|
C++ Syntax |
HRESULT get_ReverseLinearPowerLevel(double* pVal) HRESULT put_ReverseLinearPowerLevel(double newVal) |
Interface |
IGainCompression |