| Write/Read | About Segment Sweep | 
| Description | Specifies whether SA Video Bandwidth can be set independently for each segment. | 
| VB Syntax | segs.SAVectorAverageOption = value | 
| Variable | (Type) - Description | 
| segs | A Segments collection (object) | 
| value | (boolean) False - turns SA Vector Averaging control OFF. | 
| Return Type | Boolean | 
| Default | False | 
| Examples | segs.SAVectorAverageOption = True 'Write | 
| value = SAVectorAverageOption 'Read | |
| C++ Syntax | HRESULT get_SAVectorAverageOption(VARIANT_BOOL *value) HRESULT put_SAVectorAverageOption(VARIANT_BOOL value) | 
| Interface | ISegments7 |