Write/Read
About Segment Sweep

SAVideoBandwidth Property


Description

Sets or returns the SA video bandwidth.

 VB Syntax

seg.SAVideoBandwidth = value

Variable

(Type) - Description

seg

A Segment (object)

value

(Double)  Video bandwidth (in Hz).

Return Type

Double

Default

1E6 Hz

Examples

seg.SAVideoBandwidth = 1E6 'Write

value = seg.SAVideoBandwidth 'Read

C++ Syntax

HRESULT get_SAVideoBandwidth(double* pVal);

HRESULT put_SAVideoBandwidth(double pVal);

Interface

ISegment5