Read-only
About Balanced Measurements

SSB_BalPortNegative Property


Description

With a Single-ended - Single-ended - Balanced topology, returns the VNA port number that is connected to the Negative side of the DUT's Balanced Port.

Use SetSSBPorts Method to set the port mapping for a  Single-Ended - Single-Ended - Balanced topology.

 VB Syntax

var = balTopology.SSB_BalPortNegative

Variable

(Type) - Description

var

(Long Integer) Variable to store the returned value.

balTopology

A BalancedTopology (object)

Return Type

Long Integer

Default

Not Applicable

Examples

variable = balTopology.SSB_BalPortNegative  'Read

C++ Syntax

HRESULT get_SSB_BalPortNegative(long *bVal)

Interface

IBalancedTopology