Write/Read |
About Safe Sweep |
Description |
Set and read the Safe Sweep COARSE power adjustment. |
VB Syntax |
gca.SafeSweepCoarsePowerAdjustment = value |
Variable |
(Type) - Description |
gca |
A GainCompression (object) |
value |
(Double) Coarse power adjustment setting in dBm. Choose a value from +30 to (-30). |
Return Type |
Double |
Default |
3.0 |
Examples |
gca.SafeSweepCoarsePowerAdjustment = 2.0 'Write |
SSCourse = gca.SafeSweepCoarsePowerAdjustment 'Read |
|
C++ Syntax |
HRESULT get_SafeSweepCoarsePowerAdjustment(double* value) HRESULT put_SafeSweepCoarsePowerAdjustment(double value) |
Interface |
IGainCompression |