Write/Read
About Safe Sweep

SafeSweepDCParameter Property


Description

Sets and returns the name of the external DC device.

 VB Syntax

gca.SafeSweepDCParameter = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(string) - Name of the external DC device.

Return Type

String

Default

Not Applicable

Examples

gca.SafeSweepDCParameter = "MyDCDevice" 'write

value = gca.SafeSweepDCParameter 'Read

C++ Syntax

HRESULT get_SafeSweepDCParameter(BSTR* dcname)

HRESULT put_SafeSweepDCParameter(BSTR dcname)

Interface

IGainCompression6