| Write/Read | About Safe Sweep | 
| Description | Set and read the (ON | OFF) state of Safe Sweep mode. | 
| VB Syntax | gca.SafeSweepEnable = value | 
| Variable | (Type) - Description | 
| gca | A GainCompression (object) | 
| value | (Boolean) Safe Sweep state. Choose from: False - Disable Safe Sweep True - Enable Safe Sweep | 
| Return Type | Boolean | 
| Default | False | 
| Examples | gca.SafeSweepEnable = True 'Write | 
| SSEnable = gca.SafeSweepEnable 'Read | |
| C++ Syntax | HRESULT get_SafeSweepEnable(VARIANT_BOOL* value) HRESULT put_SafeSweepEnable(VARIANT_BOOL value) | 
| Interface | IGainCompression |