| Write/Read | 
| Description | This command controls the on/off state of the preference, "On PRESET show Quick Start dialog". | 
| VB Syntax | pref.ShowQuickStartOnPreset = value | 
| Variable | (Type) - Description | 
| pref | A Preferences (object) | 
| value | (Boolean) - Choose from: True - Display the Quick Start dialog on PRESET. False - Do not display the Quick Start dialog on PRESET. | 
| Return Type | Boolean | 
| Default | False | 
| Examples | pref.ShowQuickStartOnPreset = True 'Write | 
| value = pref.ShowQuickStartOnPreset 'Read | |
| C++ Syntax | HRESULT get_ShowQuickStartOnPreset (VARIANT_BOOL* preference); HRESULT put_ShowQuickStartOnPreset (VARIANT_BOOL val); | 
| Interface | IPreferences13 |