Write-only |
About Trace Statistics |
Description |
Displays and hides the measurement (Trace) statistics (peak-to-peak, mean, standard deviation) on the screen. To display measurement statistics for a narrower band of the X-axis, use StatisticsRange. The analyzer will display either measurement statistics or Filter Bandwidth statistics; not both. |
VB Syntax |
meas.ShowStatistics = value |
Variable |
(Type) - Description |
meas |
A Measurement (object) |
value |
(boolean) - Boolean value: True - Show statistics False - Hide statistics |
Return Type |
Boolean |
Default |
False |
Examples |
meas.ShowStatistics = True |
C++ Syntax |
HRESULT put_ShowStatistics(VARIANT_BOOL bState) |
Interface |
IMeasurement |