Write/Read |
About SMART Sweep |
Description |
Set and read the amount of time SMART Sweep will dwell at the first point where the input power changes by the Backoff or X level. |
VB Syntax |
gca.SmartSweepSettlingTime = value |
Variable |
(Type) - Description |
gca |
A GainCompression (object) |
value |
(double) - Settling time in seconds. Choose any positive value. |
Return Type |
Double |
Default |
0 |
Examples |
gca.SmartSweepSettlingTime = .01 'Write |
sTime = gca.SmartSweepSettlingTime 'Read |
|
C++ Syntax |
HRESULT get_SmartSweepSettlingTime(double* pVal) HRESULT put_SmartSweepSettlingTime(double newVal) |
Interface |
IGainCompression |