Write/Read
About Phase Reference Cal

SourceAttenuator Property


Description

Sets and returns the Source Attenuator setting for the Phase Reference calibration.

Note: This setting MUST match the source attenuator setting at the mixer input port for subsequent SMC+Phase measurements.

 VB Syntax

phasRef.SourceAttenuator = value

Variable

(Type) - Description

phasRef

A PhaseReferenceCalibration Object

value

Attenuation value in dB. Choose a valid value for the VNA model. See valid settings.

Return Type

Double

Default

10 dB

Examples

phase.SourceAttenuator = 0

See example program

C++ Syntax

HRESULT get_SourceAttenuator(Double* pVals);

HRESULT put_SourceAttenuator(Double pVals);

Interface

IPhaseReferenceCalibration