Write/Read | 
About SA Application | 
Description | 
 Set and read the number of SA (receiver) sweeps for each Source Step. This setting is common to all sources.  | 
VB Syntax | 
 sa.SourcePowerRepeatCount = value  | 
Variable | 
(Type) - Description | 
| 
 sa  | 
 A SpectrumAnalyzer (object)  | 
| 
 value  | 
 (Long) Repeat count. Choose an integer value of 1 or higher.  | 
Return Type | 
 Long  | 
Default | 
 1  | 
Examples | 
 sa.SourcePowerRepeatCount = 10 'Write  | 
| 
 value = sa.SourcePowerRepeatCount 'Read  | 
|
C++ Syntax | 
 HRESULT put_SourcePowerRepeatCount(long count); HRESULT get_SourcePowerRepeatCount(long* count);  | 
Interface | 
 ISpectrumAnalyzer  |