Write/Read
About SA Application

SourceStopPower Property

Description

Set and read the source stop power level. This command applies to Power or LFPower sweep types.

VB Syntax

sa.SourceStopPower (source) = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

source

(String) Source name enclosed in quotes. Use SourcePortNames to read a list of available source port names. See also Remotely Specifying a Source Port.

value

(Double) Stop power level in dBm. Choose a value within the power range of the source.

Return Type

Double

Default

Default of the source.

Examples

sa.SourceStopPower("Port 1") = 10   'Write

value = sa.SourceStopPower("Port 1") 'Read

C++ Syntax

HRESULT put_SourceStopPower(BSTR sourcename, double power);

HRESULT get_SourceStopPower(BSTR sourcename, double* power);

Interface

ISpectrumAnalyzer