Write/Read |
About SA Application |
Description |
Set and read the source sweep type. |
VB Syntax |
sa.SourceSweepType (source) = value |
Variable |
(Type) - Description |
sa |
A SpectrumAnalyzer (object) |
source |
(String) Source name enclosed in quotes. Use SourcePortNames to read a list of available source port names. See also Remotely Specifying a Source Port. |
value |
(Enum as NASweepType) Choose from: 0 - naLinearSweep - SA source sweeps from Start to Stop in linear steps. 3 - naCWTimeSweep - SA source is at a single frequency, set with SourceCWFrequency Property. |
Return Type |
Enum |
Default |
3 - naCWTimeSweep |
Examples |
sa.SourceSweepType("Port 1")= naCWTimeSweep 'Write |
value = sa.SourceSweepType("Port 1") 'Read |
|
C++ Syntax |
HRESULT put_SourceSweepType(BSTR sourcename, tagNASweepTypes sweeptype); HRESULT get_SourceSweepType(BSTR sourcename, tagNASweepTypes* sweeptype); |
Interface |
ISpectrumAnalyzer |