Read-only

 

Start Property


Description

Returns the stimulus value of the first data point for the measurement. To understand how this property is useful, see IMeasurement2 Interface.

 VB Syntax

value = meas.Start

Variable

(Type) - Description

value

(Double) - Variable to store the returned value

meas

A Measurement  (object)

Return Type

Double

Default

Not Applicable

Examples

Print meas.Start 'prints the stimulus value of the first data point

C++ Syntax

HRESULT get_Start (double * Val);

Interface

IMeasurement2