Read-only
About Embedded LO

StatusAsString Property


Description

Returns a string that describes the result of the last tuning sweeps.

 VB Syntax

value = embedLODiag.StatusAsString

Variable

(Type) - Description

value

(String) Variable to store the returned data.

embedLODiag

An EmbeddedLODiagnostic (object)

Return Type

(String)

Default

Not Applicable

Examples

data= embedLO.StatusAsString 'read

C++ Syntax

HRESULT get_StatusAsString(BSTR* status);

Interface

IEmbededLODiagnostic