Read-only
About Cal Sets

StimulusValues Property


Description

Returns the specified X-axis FOM frequency range. The array contains one frequency value for each data point.

VB Syntax

value = calSet.StimulusValues (range)

Variable

(Type) - Description

calSet

CalSet (object) - Read-only property

range

(Long) FOM frequency range to read.

0 - returns source frequencies.

1 - returns response frequencies.

2 - returns primary frequencies.

Return Type

1-dimensional variant array

Default

Not Applicable

Examples

array = CalSet.StimulusValues 'Read

C++ Syntax

HRESULT get_StimulusValues (long range, VARIANT* vals)

Interface

ICalSet3