Read-only
About CalPod as ECal

SupportsInSituCharacterization Property


Description

Returns whether the device that was specified by ECalID is a CalPod module, which is capable of being characterized as an in situ device.

VB Syntax

value = ecalUser.SupportsInSituCharacterization

Variable

(Type) - Description

value

(Boolean)

True - Device is a CalPod module

False  Device is NOT a CalPod module

ecalUser

An ECalUserCharacterizer (object)

Return Type

Boolean

Examples

Value = ecalUser.SupportsInSituCharacterization

C++ Syntax

HRESULT get_SupportsInSituCharacterization(VARIANT_BOOL *value);

Interface

IECalUserCharacterizer3