Read/Write

SweepEndMode Property


Description

Sets and reads the event that will cause the Sweep End line to go to a low state. The line will return to a high state after the appropriate calculations are complete.

Note: This line is connected to the HANDLER IO connector.

 VB Syntax

object.SweepEndMode = value

Variable

(Type) - Description

object

(object) - A HandlerIO or AuxIO object

value

(enum as NASweepEndMode ) Choose from:

0 - naSweep - the line goes low when each sweep is complete

1 - naChannelSweep - the line goes low when all the sweeps for each channel is complete.

2 - naGlobalSweep - the line goes low when all sweeps for all triggerable channels are complete.

Return Type

Long Integer

Default

0 - naSweep

Examples

HWAuxIO.PassFailMode = naSweep 'Write

value = HWAuxIO.PassFailMode 'Read

C++ Syntax

HRESULT put_SweepEndMode ( tagNASweepEndMode Mode );

HRESULT get_SweepEndMode ( tagNASweepEndMode* Mode );

Interface

IHWAuxIO

IHWMaterialHandlerIO