Write/Read | 
		About Segment Sweep | 
	
Description | 
		Enables or disables sweep mode per segment. Value is set using the SweepMode Property of a Segment.  | 
	
VB Syntax | 
		segs.SweepModeOption = value  | 
	
Variable | 
		(Type) - Description | 
	
segs  | 
		A Segments collection (object)  | 
	
value  | 
		(boolean) False - Disable sweep mode.  | 
	
Return Type | 
		Boolean  | 
	
Default | 
		False  | 
	
Examples | 
		segs.SweepModeOption = True 'Write  | 
	
sweepstate = segs.SweepModeOption 'Read  | 
	|
C++ Syntax | 
		HRESULT get_SweepModeOption(VARIANT_BOOL* pVal) HRESULT put_SweepModeOption(VARIANT_BOOL pVal)  | 
	
Interface | 
		ISegments6  |