Write/Read
About Modifying Cal Kits

TZImag Property


Description

Sets and Returns the TZImag value (the Imaginary Terminal Impedance value) for the calibration standard. Only applicable when "Type" is set to naArbitraryImpedance.

To set the other resistance values, use TZReal

 VB Syntax

calstd.TZImag = value

Variable

(Type) - Description

calstd

A CalStandard (object). Use calKit.GetCalStandard to get a handle to the standard.

value

(single) - Value for TZImag in Ohms

Return Type

Single

Default

Not Applicable

Examples

calstd.TZImag = 15 'Write the value of TZImag to 15 Ohms

imp0 = calstd.TZImag 'Read the value of TZImag

C++ Syntax

HRESULT get_TZImag(float *pVal);
HRESULT put_TZImag(float newVal);

Interface

ICalStandard2