Read-only
About External Testset Control

TestSetType Property


Description

Returns the Test Set Type (model) that was used for the Cal Set.

 VB Syntax

TSType = calset.TestSetType

Variable

(Type) - Description

TSType

(String)  Variable to store the returned test set model.

calset

A  Cal Set object.

Return Type

String

Default

Depends on the test set.

Example

TSType = calset.TestSetType

C++ Syntax

HRESULT get_OutputPorts(BSTR *mapping);

Interface

ICalset5