Read/Write
Learn about Calibration Thru Methods

ThruCalMethod Property  Superseded


Description

This command is replaced by PathThruMethod Property.

Sets and returns the method for performing the Cal Method and the THRU portion of the calibration.

VB Syntax

guidedCal.ThruCalMethod = value

Variable

(Type) - Description

guidedCal

GuidedCalibration (object)

value

(Enum as NAThruCalMethod)  Choose from:

0 - naDefaultCalMethod - allow the VNA to choose the best possible method (from the following) depending on whether the device or ECal module is insertable or non-insertable and given the model number of the VNA. (default selection if omitted.)

1 - naAdapterRemoval - Perform Adapter removal calibration.

2 - naFlushThru - Perform Flush Thru calibration.

3 - naDefinedThru - Perform Defined Thru calibration. If performing an ECal, this is the Thru standard in the ECal module.

4 - naUnknownThru - Perform Unknown Thru calibration.

5 - naSOLT - Perform SOLT calibration

6 - naTRL - Perform TRL calibration

7 - naQSOLT - Perform QSOLT calibration.

Learn more about Cal Methods

Return Type

Enum

Default

0 - naDefaultCalMethod

Examples

guided.ThruCalMethod = naDefinedThru

C++ Syntax

HRESULT get_ThruCalMethod(enum NAThruCalMethod *thruMethod);

HRESULT put_ThruCalMethod(enum NAThruCalMethod thruMethod);

Interface

IGuidedCalibration