| Write/Read | About External Devices | 
| Description | Sets and returns the Time out value for communication with the external device. An error is returned if communication with the device is not successful within this period of time. | 
| VB Syntax | extDevices.TimeOut = value | 
| Variable | (Type) - Description | 
| extDevices | An ExternalDevice (object) | 
| value | (Double) Time out in milliseconds. | 
| Return Type | Double | 
| Default | 20000 milliseconds (20 seconds) | 
| Examples | extDevices.TimeOut = 1000 Write value = extDevices.TimeOut 'Read | 
| C++ Syntax | HRESULT get_TimeOut(Double* value); HRESULT put_TimeOut(Double newVal); | 
| Interface | IExternalDevices |