Write/Read |
About Trace Title |
Description |
Writes and reads data for the trace title area. The trace title is embedded in the trace status field. Learn more about Trace Titles The title is turned ON and OFF using TraceTitleState. |
VB Syntax |
meas.TraceTitle = value |
Variable |
(Type) - Description |
meas |
A Measurement (object) |
value |
(string) - Title to be displayed. Any characters (no spaces), enclosed with quotes. |
Return Type |
String |
Default |
Not Applicable |
Examples |
meas.TraceTitle = "My new s11 measurement" |
title = TraceTitle 'Read |
|
C++ Syntax |
HRESULT get_TraceTitle(BSTR *title ); |
Interface |
IMeasurement8 |