Write/Read
About Triggering ADC

TriggerADCLevelState Property


Description

Set and read the ON/OFF state of a measurement trigger event that will occur whenever the ADC level is greater than the value specified using the TriggerADCLevelValue command.

VB Syntax

sa.TriggerADCLevelState = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Boolean) Choose from:

0 - OFF - ADC measurement trigger OFF.

1 - ON - ADC measurement trigger ON.

Learn about these settings.

Return Type

Boolean

Default

0

Examples

sa.TriggerADCLevelState = OFF   Write

value = sa.TriggerADCLevelState 'Read

See an example program.

C++ Syntax

HRESULT put_TriggerADCLevelState(VARIANT_BOOL bEnable);

HRESULT get_TriggerADCLevelState(VARIANT_BOOL* bEnable);

Interface

ISpectrumAnalyzer