| Write/Read | About Triggering ADC | 
| Description | Set and read the ADC trigger level. | 
| VB Syntax | sa.TriggerADCLevelValue = value | 
| Variable | (Type) - Description | 
| sa | A SpectrumAnalyzer (object) | 
| value | (Long) Choose a value between 0 and 16383. | 
| Return Type | Long | 
| Default | 100 | 
| Examples | sa.TriggerADCLevelValue = 256 'Write | 
| value = sa.TriggerADCLevelValue 'Read | |
| C++ Syntax | HRESULT put_TriggerADCLevelValue(long val); HRESULT get_TriggerADCLevelValue(long* val); | 
| Interface | ISpectrumAnalyzer |