Write/Read
About Ext DC Devices

TriggerInPin Property


Description

When Trigger mode is set to Hardware List for SMU devices, this command sets and returns the B2900 Digital IO pin to use for Trigger IN.

 VB Syntax

extDC.TriggerInPin = value

Variable

(Type) - Description

extDC

An ExternalDCDevice (object)

value

(Long) Pin number for Trigger IN. Choose a pin number from 1 to 14.

Return Type

Long

Default

1

Examples

extDC.TriggerInPin = 3 'Write

bool = extDC.TriggerInPin 'Read

C++ Syntax

HRESULT get_TriggerInPin (Long *pValue)

HRESULT put_TriggerInPin (long newVal)

Interface

IExternalDCDevice2