Write/Read |
About ExternalDevices |
Description |
Sets and returns the trigger mode for an external source. |
VB Syntax |
extSource.TriggerMode = value |
Variable |
(Type) - Description |
extSource |
An ExternalSource Object (object) |
value |
(enum NAExtDevTriggerMode) - Choose from: 0 - naExtDevTriggerModeCW 1 - naExtDevTriggerModeHW |
Return Type |
Enum |
Default |
0 - naExtDevTriggerModeCW |
Examples |
extSource.TriggerMode = naExtDevTriggerModeCW 'Write |
tm = extSource.TriggerMode 'Read |
|
C++ Syntax |
HRESULT get_TriggerMode (tagNAExtDevTriggerMode *pMode) |
Interface |
IExternalSource |