Write/Read
About Auxiliary Triggering

TriggerOutInterval Property


Description

Specifies how often a trigger output signal is sent.

 VB Syntax

auxTrig.TriggerOutInterval = value

Variable

(Type) - Description

auxTrig

An AuxTrigger (object)

value

(single) - Choose from:

0 - naTriggerModePoint - a single data point is measured with each trigger signal the channel receives. Subsequent trigger signals continue to go to the channel in Point mode until the channel measurements are complete. This is effectively the same as trigger point mode.

1 - naTriggerModeMeasurement - entire traces are swept with a trigger signal. which and how many traces depends on the Scope setting.

Return Type

Enum

Default

1 - naTriggerModeMeasurement

Exaamples

auxTrig.TriggerOutInterval = naTriggerModeMeasurement 'Write

value = auxTrig.TriggerOutInterval 'Read the value

C++ Syntax

HRESULT get_TriggerOutInterval(enum NATriggerMode *val);
HRESULT put_TriggerOutInterval(enum NATriggerMode val);

Interface

IAuxTrigger