Write/Read
About Auxiliary Triggering

TriggerOutPosition Property


Description

Specifies whether the Aux trigger out signal is sent Before or After the acquisition.

 VB Syntax

auxTrig.TriggerOutPosition = value

Variable

(Type) - Description

auxTrig

An AuxTrigger (object)

value

(enum NATriggerPosition) Choose from:

naTriggerOutBeforeAcquire  Use if the external device needs to be triggered before the data is acquired, such as a power meter.

naTriggerOutAfterAcquire  Use if the external device needs to be triggered just after data has been acquired, such as an external source. This could be more efficient since it allows the external device to get ready for the next acquisition at the same time as the VNA.

Return Type

Enum

Default

naTriggerOutAfterAcquire

Exaamples

auxTrig.TriggerOutPosition = naTriggerOutAfterAcquire 'Write

value = auxTrig.TriggerOutPosition 'Read the value

C++ Syntax

HRESULT get_TriggerOutPosition(enum NATriggerPosition *val);
HRESULT put_TriggerOutPosition(NATriggerPosition val);

Interface

IAuxTrigger