Write/Read |
About Periodic Counter |
Description |
Set and read the periodic counter value. This command initiates a measurement trigger event based on the specified period. |
VB Syntax |
sa.TriggerPeriodicCounterValue = value |
Variable |
(Type) - Description |
sa |
A SpectrumAnalyzer (object) |
value |
(Long) Choose a value between 0 and 2147483647. |
Return Type |
Long |
Default |
256 |
Examples |
sa.TriggerPeriodicCounterValue = 256 'Write |
value = sa.TriggerPeriodicCounterValue 'Read |
|
C++ Syntax |
HRESULT put_TriggerPeriodicCounterValue(long val); HRESULT get_TriggerPeriodicCounterValue(long* val); |
Interface |
ISpectrumAnalyzer |