Read/Write |
About Embedded LO |
Description |
Set the IF Bandwidth for Broadband and Precise tuning sweeps. |
VB Syntax |
obj.TuningIFBW = value |
Variable |
(Type) - Description |
obj |
An EmbeddedLO (object) or A ConverterEmbeddedLO (object) |
value |
(Double) IF Bandwidth |
Return Type |
(Double) |
Default |
30 kHz |
Examples |
embedLO.TuningIFBW = 10e3 'write |
value = embedLO.TuningIFBW 'read |
|
C++ Syntax |
HRESULT get_TuningIFBW(double* ifbw); HRESULT put_TuningIFBW(double ifbw); |
Interface |
IEmbededLO |