Read/Write
About Embedded LO

TuningSweepInterval Property


Description

Set how often a tuning sweep is performed.

 VB Syntax

obj.TuningSweepInterval = value

Variable

(Type) - Description

obj

An EmbeddedLO (object) or

A ConverterEmbeddedLO (object)

value

(Long) Tuning sweep interval.

Return Type

(Long)

Default

1

Examples

embedLO.TuningSweepInterval = 3 'write .. tuning is performed every third measurement sweep

value = embedLO.TuningSweepInterval 'read

C++ Syntax

HRESULT get_TuningSweepInterval(long* interval);

HRESULT put_TuningSweepInterval(long interval);

Interface

IEmbededLO