Write/Read |
About Group Delay |
Description |
Sets the default group delay aperture setting. |
VB Syntax |
pref.TwoPointGroupDelayAperture = value |
Variable |
(Type) - Description |
pref |
A Preferences (object) |
value |
(Boolean) - Choose from: True - Set the default group delay aperture setting to two points. False - Set the default group delay aperture setting to 11 points. |
Return Type |
Boolean |
Default |
False |
Examples |
pref.TwoPointGroupDelayAperture = True 'Write |
gda = pref.TwoPointGroupDelayAperture 'Read |
|
C++ Syntax |
HRESULT get_TwoPointGroupDelayAperture(VARIANT_BOOL* pVal); |
Interface |
IPreferences11 |