Write/Read |
About Source Power CalAbout PMAR |
Description |
Sets and returns a custom model uncertainty file containing all of the power meter uncertainty properties. When this command is executed, the model name is automatically set to "CustomFile". |
VB Syntax |
pwrSensor.UncertaintyFile = value |
Variable |
(Type) - Description |
pwrSensor |
A PowerSensorUncertainty (Object) |
value |
(String) -Custom file name. |
Return Type |
String |
Default |
Not Applicable |
Examples |
pwrSensor.UncertaintyFile = "C:\U8485A_MY55140018.dat" 'Write value = pwrSensor.UncertaintyFile 'Read |
C++ Syntax |
HRESULT put_UncertaintyFile(BSTR *pVal); HRESULT get_UncertaintyFile(BSTR pVal); |
Interface |
IPowerSensorUncertainty |