Write/Read
About Phase Reference Cals

UnknownMixerInputPower Property


Description

Sets and returns the input power level to the unknown mixer.

 VB Syntax

phaseRef.UnknownMixerInputPower = value

Variable

(Type) - Description

object

PhaseReferenceCalibration (object)

value

(Double) Input power level in dBm.

Return Type

Double

Default

-15 dBm

Examples

phaseRef.UnknownMixerInputPower = 0

value = phaseRef.UnknownMixerInputPower 'Read

C++ Syntax

HRESULT get_UnknownMixerInputPower(double *value)

HRESULT put_UnknownMixerInputPower(double value)

Interface

IPhaseReference2