Write/Read |
About Phase Reference Cals |
Description |
Sets and returns the LO power level to the unknown mixer. |
VB Syntax |
phaseRef.UnknownMixerLOPower = value |
Variable |
(Type) - Description |
object |
PhaseReferenceCalibration (object) |
value |
(Double) LO power level in dBm. |
Return Type |
Double |
Default |
10 dBm |
Examples |
phaseRef.UnknownMixerLOPower = 10 |
value = phaseRef.UnknownMixerLOPower 'Read |
|
C++ Syntax |
HRESULT get_UnknownMixerLOPower(double *value) HRESULT put_UnknownMixerLOPower(double value) |
Interface |
IPhaseReference2 |