Read-only
 

UnusedChannelNumbers Property


Description

Returns an array of channel numbers that are NOT in use. An unused channel has NO measurements subscribed to it.

VB Syntax

chanNumbers = chans.UnusedChannelNumbers (NumberOfChannels)

Variable

(Type) - Description

chanNumbers

Variable array to store the returned channel numbers

chans

A Channel collection (object)

NumberOfChannels

(Long Integer) Number of channels that you are requesting.

Return Type

One-dimensional array of long integers. The size of the array is specified by the NumberOfChannels parameter.

Default

Not Applicable

Examples

chanNumbers = chans.UnusedChannelNumbers(5)

C++ Syntax

HRESULT get_UnusedChannelNumbers(long numberRequested,VARIANT* channelNumbers);

Interface

IChannels2