Write / Read
About Source Power Cal
About PMAR

UsePowerLossSegments Property


Description

Specifies if subsequent power readings will use of the loss table. (PowerLossSegments).

 VB Syntax

pwrCal.UsePowerLossSegments = value

Variable

(Type) - Description

pwrCal

A SourcePowerCalibrator (object)

A PowerSensorAsReceiver (Object)

A PowerSensor (Object)

value

(boolean)

False – Do not use loss table

True – Use loss table

Return Type

Boolean

Default

False

Examples

pwrSens.UsePowerLossSegments = True 'Write
lossTableState = pwrSens.UsePowerLossSegments 'Read

C++ Syntax

HRESULT put_UsePowerLossSegments(VARIANT_BOOL bState);

HRESULT get_UsePowerLossSegments(VARIANT_BOOL *bState);

Interface

ISourcePowerCalibrator

IPowerSensorAsReceiver

IPowerSensor