Write/Read
About User Ranges

UserRangeMin Property


Description

Sets the stimulus start value for the specified User Range.

This property uses different arguments for the channel and marker objects.

 VB Syntax

chan.UserRangeMin(domainType,range) = value

or

mark.UserRangeMin(range) = value

Variable

(Type) - Description

chan

A Channel (object)

mark

A Marker (object)

To assign a marker to a User Range, use the UserRange Property.

domainType

Note: The Marker object does not require the domainType argument.

(enum NADomainType) Type of sweep currently implemented on the channel - Choose from:

0 - naDomainFrequency

1 - naDomainTime

2 - naDomainPower

3 - naDomainPhase

  range

(long) - User Range number. Choose any number between 1 and 16 (0=Full Span)

value

(double) - Start value. Choose any number within the full span of the analyzer

Return Type

Double

Default

The current stimulus setting for the channel

Examples

mark.UserRangeMin(1) = 3e9 'Write
chan.UserRangeMin(naDomainFrequency,1) = 3e9 'Write

UseRngeMin = mark.UserRangeMin 'Read
UseRngeMin = chan.UserRangeMin 'Read

C++ Syntax

HRESULT put_UserRangeMin(tagNADomainType domain, long rangeNumber, double minValue)
HRESULT get_UserRangeMin(tagNADomainType domain, long rangeNumber, double *minValue)

Interface

IChannel