Read-only
About Equation Editor

Valid Property


Description

Returns a boolean value to indicate if the current equation on the measurement is valid. For equation processing to occur, the equation must be valid and ON.

 VB Syntax

IsValid = eq.Valid

Variable

(Type) - Description

good

(Boolean) Variable to store the returned value.

True (1) - equation is valid

False (0) - equation is NOT valid

eq

MeasurementEquation (object)

Return Type

Boolean

Default

Not Applicable

Examples

IsValid = eq.Valid 'Read

C++ Syntax

HRESULT get_Valid(Boolean *equation)

Interface

IMeasurementEquation