Write/Read
About SA Application

VideoAveragingType Property


Description

Set and read the video averaging type.

VB Syntax

sa.VideoAveragingType = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Enum as NASAVideoAveragingType) Choose from:

0 - naPower

1 - naLog

2 - naVoltage

3 - naVoltageMax

4 - naVoltageMin

Learn about these settings.

Return Type

Enum

Default

0 - naPower

Examples

sa.VideoAveragingType = naLog   'Write

value = sa.VideoAveragingType 'Read

See an example program.

C++ Syntax

HRESULT put_VideoAveragingType(tagNASAVideoAveragingType type);

HRESULT get_VideoAveragingType(tagNASAVideoAveragingType* type);

Interface

ISpectrumAnalyzer