Write/Read |
About SA Application |
Description |
Set and read how the video bandwidth is set. When ON, video bandwidth is set based on RBW/VBW ratio. |
VB Syntax |
sa.VideoBWMode = value |
Variable |
(Type) - Description |
sa |
A SpectrumAnalyzer (object) |
value |
(Enum as NAModes) Choose from: 1 - naMANUAL - Video BW is set manually using VideoBW Property 0 - naAUTO - Video BW is set automatically. |
Return Type |
Enum |
Default |
0 - naAUTO |
Examples |
sa.VideoBWMode = naMANUAL Write |
value = sa.VideoBWMode 'Read |
|
C++ Syntax |
HRESULT put_VideoBWMode(tagNAModes mode); HRESULT get_VideoBWMode(tagNAModes* mode); |
Interface |
ISpectrumAnalyzer |