| Write/Read | About X-Axis Spacing | 
| Description | Sets X-axis Point Spacing for the displaytraces measured with segment sweeps on the active channel. | 
| VB Syntax | chan.XAxisPointSpacing = value | 
| Variable | (Type) - Description | 
| chan | A Channel (object) | 
| value | (Enum as naStates) - Choose from: 0 - naOFF - Turns X-axis Point Spacing OFF 1 - naON - Turns X-axis Point Spacing ON | 
| Return Type | Enum | 
| Default | 0 - naOFF | 
| Examples | chan.XAxisPointSpacing = naOFF 'Write | 
| xspac = chan.XAxisPointSpacing 'Read | |
| C++ Syntax | HRESULT get_XAxisPointSpacing (tagNAStates *pState); | 
| Interface | IChannel2 |