Read-only |
About Diff I/Q App |
Description |
Returns the X-Axis source of the selected measurement. See Also: |
VB Syntax |
src = DIQMeas.XAxisSource |
Variable |
(Type) - Description |
src |
(String) - Variable to store the returned source for the domain that is displayed on the X-axis. See ActiveXAxis Property for possible returned values. |
DIQMeas |
A DIQMeas (object) |
Example |
src = diqMeas.XAxisSource 'Read 'Returns "Port 1" |
C++ Syntax |
HRESULT get_XAxisSource(BSTR* source); |
Interface |
IDIQMeas |